sl_bt_evt_sync_closedSynchronization#
Indicates that periodic advertising synchronization was lost or a synchronization establishment procedure was canceled.
Data Structures#
struct | Data structure of the closed event. |
Macros#
#define | sl_bt_evt_sync_closed_id 0x014200a0 Identifier of the closed event. |
Detailed Description#
Indicates that periodic advertising synchronization was lost or a synchronization establishment procedure was canceled.
The synchronization establishment procedure can be canceled explicitly by the application by issuing command sl_bt_sync_close, or internally due to synchronization failing. Synchronization can fail for example due to incompatible sync CTE type.
Data Structure Documentation#
sl_bt_evt_sync_closed_s#
struct sl_bt_evt_sync_closed_s
Data structure of the closed event.
Data Fields | ||
|---|---|---|
uint16_t | reason | Result code
|
uint16_t | sync | Periodic advertising synchronization handle |