sl_bt_evt_sm_confirm_bondingSecurity Manager#
Indicates a user request to display that the new bonding request is received and for the user to confirm the request.
Data Structures | |
|---|---|
struct | |
Data structure of the confirm_bonding event. More... | |
Macros | |
|---|---|
#define | sl_bt_evt_sm_confirm_bonding_id 0x090f00a0 |
Identifier of the confirm_bonding event. | |
Detailed Description#
Indicates a user request to display that the new bonding request is received and for the user to confirm the request.
Use the command sl_bt_sm_bonding_confirm to accept or reject the bonding request.
Data Structure Documentation#
sl_bt_evt_sm_confirm_bonding_s#
struct sl_bt_evt_sm_confirm_bonding_s
Data structure of the confirm_bonding event.
Data Fields | ||
|---|---|---|
uint8_t | connection | Connection handle |
uint8_t | bonding_handle | Bonding handle for the request. Range: 0 to 31, or SL_BT_INVALID_BONDING_HANDLE (0xff).* NOTE! When the bonding handle is anything other than SL_BT_INVALID_BONDING_HANDLE (0xff), a bonding already exists for this connection. Overwriting the existing bonding is a potential security risk. |