sl_bt_evt_system_external_signalSystem#
Indicates that the external signals have been received.
Data Structures | |
struct | |
Data structure of the external_signal event. | |
Macros | |
# define | sl_bt_evt_system_external_signal_id 0x030100a0 |
Identifier of the external_signal event. | |
Detailed Description#
Indicates that the external signals have been received.
External signals are generated from the native application.
Data Structure Documentation#
sl_bt_evt_system_external_signal_s#
struct sl_bt_evt_system_external_signal_s |
Data structure of the external_signal event.
Data Fields | |
|---|---|
uint32_t | |
extsignals | Bitmask of external signals received since last event. |