sl_bt_evt_system_errorSystem#
Indicates that an error has occurred.
Data Structures | |
struct | |
Data structure of the error event. | |
Macros | |
# define | sl_bt_evt_system_error_id 0x060100a0 |
Identifier of the error event. | |
Detailed Description#
Indicates that an error has occurred.
See error codes table for more information.
Data Structure Documentation#
sl_bt_evt_system_error_s#
struct sl_bt_evt_system_error_s |
Data structure of the error event.
Data Fields | |
|---|---|
uint16_t | |
reason | Result code* 0: success |
Non-zero: an error has occurred | | uint8array | data | Data related to the error; this field can be empty. |