sl_bt_evt_connection_get_remote_tx_power_completedConnection#
Indicates that reading remote transmit power initiated by sl_bt_connection_get_remote_tx_power command has completed.
Data Structures#
struct | sl_bt_evt_connection_get_remote_tx_power_completed_s Data structure of the get_remote_tx_power_completed event. |
Macros#
#define | sl_bt_evt_connection_get_remote_tx_power_completed_id 0x050600a0 Identifier of the get_remote_tx_power_completed event. |
Detailed Description#
Indicates that reading remote transmit power initiated by sl_bt_connection_get_remote_tx_power command has completed.
Data Structure Documentation#
sl_bt_evt_connection_get_remote_tx_power_completed_s#
struct sl_bt_evt_connection_get_remote_tx_power_completed_s
Data structure of the get_remote_tx_power_completed event.
Data Fields | ||
|---|---|---|
uint16_t | status | SL_STATUS_OK or another error code indicating the reading remote transmit power operation failed. |
uint8_t | connection | Handle of the connection |
uint8_t | phy | Enum sl_bt_gap_phy_and_coding_type_t. The PHY for which the transmit power is reported. Values:
|
int8_t | power_level | Transmit power level. Values: Range -127 to 20: The transmit power level in dBm SL_BT_CONNECTION_TX_POWER_UNMANAGED (0x7E): Remote device is not managing power levels on this PHY. SL_BT_CONNECTION_TX_POWER_UNAVAILABLE (0x7F): Transmit power level is not available. |
uint8_t | flags | Enum sl_bt_connection_tx_power_flag_t. Transmit power level flags. Ignore this field if
|
int8_t | delta | Change in transmit power level. Values:
|