Data structure of the server_status_period event.
Public Attribute Documentation#
client_address#
uint16_t sl_btmesh_evt_health_client_server_status_period_s::client_address
Destination address the message was sent to
Definition at line
4573
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_health_client_server_status_period_s::elem_index
Client model element index. Identifies the client model, which received the status message.
Definition at line
4574
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_health_client_server_status_period_s::server_address
Address of the Server model which sent the message
Definition at line
4576
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
result#
uint16_t sl_btmesh_evt_health_client_server_status_period_s::result
Response status. If an error occurs (e.g., request timeout), ignore the parameters other than element index, client address, and server address.
Definition at line
4578
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
period#
uint8_t sl_btmesh_evt_health_client_server_status_period_s::period
Health period divisor value
Definition at line
4582
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h