Data structure of the light_onoff_status event.
Public Attribute Documentation#
destination_address#
uint16_t sl_btmesh_evt_lc_client_light_onoff_status_s::destination_address
Address of the client or the group address to which it was published.
Definition at line
13544
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_lc_client_light_onoff_status_s::elem_index
Index of the element for which received the status.
Definition at line
13546
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_lc_client_light_onoff_status_s::server_address
Device which sent the status.
Definition at line
13548
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_lc_client_light_onoff_status_s::appkey_index
Appkey used by server_address.
Definition at line
13549
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
present_light_onoff#
uint8_t sl_btmesh_evt_lc_client_light_onoff_status_s::present_light_onoff
Present value of the Light OnOff state
Definition at line
13550
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
target_light_onoff#
uint8_t sl_btmesh_evt_lc_client_light_onoff_status_s::target_light_onoff
Target value of the Light OnOff state
Definition at line
13551
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
remaining_time_ms#
uint32_t sl_btmesh_evt_lc_client_light_onoff_status_s::remaining_time_ms
Time (in milliseconds) remaining in transition
Definition at line
13552
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h