Data structure of the property_status event.

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_lc_client_property_status_s::destination_address

Address of the client or the group address to which it was published.


Definition at line 13576 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_lc_client_property_status_s::elem_index

Index of the element for which received the status.


Definition at line 13578 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_lc_client_property_status_s::server_address

Device which sent the status.


Definition at line 13580 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_lc_client_property_status_s::appkey_index

Appkey used by server_address.


Definition at line 13581 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

property_id#

uint16_t sl_btmesh_evt_lc_client_property_status_s::property_id

Property ID


Definition at line 13582 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

property_value#

uint8array sl_btmesh_evt_lc_client_property_status_s::property_value

Property value


Definition at line 13583 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h