Data structure of the data_header event.
Public Attribute Documentation#
handle#
uint32_t sl_btmesh_evt_lcd_client_data_header_s::handle
Request handle
Definition at line
21660
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
page_number#
uint8_t sl_btmesh_evt_lcd_client_data_header_s::page_number
Page number of the Composition Data
Definition at line
21661
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
offset#
uint16_t sl_btmesh_evt_lcd_client_data_header_s::offset
Offset within the page
Definition at line
21662
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
total_size#
uint16_t sl_btmesh_evt_lcd_client_data_header_s::total_size
Total size of the page
Definition at line
21663
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h