Data structure of the partial_block_report_tx_complete event.

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_mbt_server_partial_block_report_tx_complete_s::elem_index

The server model element index.


Definition at line 11412 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

num_requested_chunks#

uint16_t sl_btmesh_evt_mbt_server_partial_block_report_tx_complete_s::num_requested_chunks

Number of requested chunks.


Definition at line 11413 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

requested_chunks#

uint8array sl_btmesh_evt_mbt_server_partial_block_report_tx_complete_s::requested_chunks

The array of requested chunks in little-endian uint16 format.


Definition at line 11414 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h