Data structure of the fw_deleted event.

Public Attributes#

uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_ncp_fw_list_fw_deleted_s::elem_index

Server model element index


Definition at line 20206 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_ncp_fw_list_fw_deleted_s::client_address

Address of the Distribution Client


Definition at line 20207 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

fwid#

uint8array sl_btmesh_evt_ncp_fw_list_fw_deleted_s::fwid

FWID of the firmware that was deleted


Definition at line 20208 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h