Data structure of the gatt_proxy_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_private_beacon_client_gatt_proxy_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
21378
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
handle#
uint32_t sl_btmesh_evt_private_beacon_client_gatt_proxy_status_s::handle
Request handle
Definition at line
21379
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
state#
uint8_t sl_btmesh_evt_private_beacon_client_gatt_proxy_status_s::state
Private gatt proxy beacon state of the node. Valid values are:
0: Node is not broadcasting private gatt proxy beacons
1: Node is broadcasting private gatt proxy beacons
Definition at line
21380
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h