Data structure of the extended_scan_report event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_remote_provisioning_client_extended_scan_report_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
19250
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server#
uint16_t sl_btmesh_evt_remote_provisioning_client_extended_scan_report_s::server
Server address.
Definition at line
19252
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
status#
uint8_t sl_btmesh_evt_remote_provisioning_client_extended_scan_report_s::status
Enum sl_btmesh_remote_provisioning_server_status_t. server status.
Definition at line
19253
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
uuid#
uuid_128 sl_btmesh_evt_remote_provisioning_client_extended_scan_report_s::uuid
UUID of the unprovisioned device found
Definition at line
19256
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
oob#
uint16_t sl_btmesh_evt_remote_provisioning_client_extended_scan_report_s::oob
OOB information. 0 if not present
Definition at line
19257
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
ad_structures#
uint8array sl_btmesh_evt_remote_provisioning_client_extended_scan_report_s::ad_structures
Concatenated list of AD Structures that match the AD Types requested by the client.
Definition at line
19258
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h