Data structure of the link_report event.

Public Attributes#

uint16_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

server#

uint16_t sl_btmesh_evt_remote_provisioning_client_link_report_s::server

Server address.


Definition at line 19310 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

status#

uint8_t sl_btmesh_evt_remote_provisioning_client_link_report_s::status

Enum sl_btmesh_remote_provisioning_server_status_t. server status.


Definition at line 19311 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

state#

uint8_t sl_btmesh_evt_remote_provisioning_client_link_report_s::state

Enum sl_btmesh_remote_provisioning_client_link_state_t. link state.


Definition at line 19313 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

reason#

uint8_t sl_btmesh_evt_remote_provisioning_client_link_report_s::reason

0: success, 1: procedure timeout 2:procedure failed, 0xff not available.


Definition at line 19316 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h