Data structure of the link_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_remote_provisioning_client_link_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
19280
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server#
uint16_t sl_btmesh_evt_remote_provisioning_client_link_status_s::server
Server address.
Definition at line
19281
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
status#
uint8_t sl_btmesh_evt_remote_provisioning_client_link_status_s::status
Enum sl_btmesh_remote_provisioning_server_status_t. server status.
Definition at line
19282
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
state#
uint8_t sl_btmesh_evt_remote_provisioning_client_link_status_s::state
Enum sl_btmesh_remote_provisioning_client_link_state_t. link state.
Definition at line
19284
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h