Data structure of the scan_report event.
Public Attribute Documentation#
server#
uint16_t sl_btmesh_evt_remote_provisioning_client_scan_report_s::server
Server address.
Definition at line
19221
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
rssi#
int8_t sl_btmesh_evt_remote_provisioning_client_scan_report_s::rssi
measured signal stength in dBm.
Definition at line
19222
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
uuid#
uuid_128 sl_btmesh_evt_remote_provisioning_client_scan_report_s::uuid
UUID of the unprovisioned device found
Definition at line
19223
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
oob#
uint16_t sl_btmesh_evt_remote_provisioning_client_scan_report_s::oob
OOB information.
Definition at line
19224
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
uri#
uint32_t sl_btmesh_evt_remote_provisioning_client_scan_report_s::uri
Hash of the out-of-band URI, which is received in a separate event . If the URI bit (bit 1) is not set in the OOB capabilities bitfield, this field is ignored.
Definition at line
19225
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h