Data structure of the store event.
Public Attribute Documentation#
destination_address#
uint16_t sl_btmesh_evt_scene_setup_server_store_s::destination_address
Address of the server or the group address to which it was published.
Definition at line
14910
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_scene_setup_server_store_s::elem_index
Index of the element which received the command.
Definition at line
14912
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
scene_id#
uint16_t sl_btmesh_evt_scene_setup_server_store_s::scene_id
Scene ID
Definition at line
14914
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_scene_setup_server_store_s::client_address
Device which sent the request.
Definition at line
14915
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_scene_setup_server_store_s::appkey_index
Appkey used by client_address.
Definition at line
14916
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h