Data structure of the status event.
Public Attribute Documentation#
client_address#
uint16_t sl_btmesh_evt_scheduler_client_status_s::client_address
Destination client model address
Definition at line
15030
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_scheduler_client_status_s::elem_index
Client model element index
Definition at line
15031
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_scheduler_client_status_s::server_address
Source server model address
Definition at line
15032
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_scheduler_client_status_s::appkey_index
The application key index to use.
Definition at line
15033
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
scheduler#
uint16_t sl_btmesh_evt_scheduler_client_status_s::scheduler
Bit field indicating defined Actions in the Schedule Register
Definition at line
15034
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h