Data structure of the publish event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_sensor_client_publish_s::elem_index
Client model element index
Definition at line
12652
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
period_ms#
uint32_t sl_btmesh_evt_sensor_client_publish_s::period_ms
The current publishing period that can be used to estimate the next tick, e.g., when the state should be reported at higher frequency.
Definition at line
12653
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h