Data structure of the settings_status event.

Public Attributes#

uint16_t
uint16_t
uint8_t
uint16_t

Public Attribute Documentation#

client_address#

uint16_t sl_btmesh_evt_sensor_client_settings_status_s::client_address

Destination client model address


Definition at line 12441 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_sensor_client_settings_status_s::elem_index

Client model element index


Definition at line 12442 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_sensor_client_settings_status_s::server_address

Source server model address


Definition at line 12443 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_sensor_client_settings_status_s::appkey_index

The application key index to use


Definition at line 12444 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

flags#

uint8_t sl_btmesh_evt_sensor_client_settings_status_s::flags

No flags defined currently


Definition at line 12445 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

property_id#

uint16_t sl_btmesh_evt_sensor_client_settings_status_s::property_id

Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.


Definition at line 12446 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

setting_ids#

uint8array sl_btmesh_evt_sensor_client_settings_status_s::setting_ids

Array of 16-bit Setting Property IDs of the settings the given sensor has


Definition at line 12449 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h