Data structure of the model_status event.

Public Attributes#

uint16_t
uint8_t
uint8_t
uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

server#

uint16_t sl_btmesh_evt_silabs_config_client_model_status_s::server

Server address.


Definition at line 3846 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

status#

uint8_t sl_btmesh_evt_silabs_config_client_model_status_s::status

Enum sl_btmesh_silabs_config_client_status_t. Status code from the Server.


Definition at line 3847 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint8_t sl_btmesh_evt_silabs_config_client_model_status_s::elem_index

Element index of model to configure.


Definition at line 3849 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

vendor_id#

uint16_t sl_btmesh_evt_silabs_config_client_model_status_s::vendor_id

Vendor ID of model to configure.


Definition at line 3850 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

model_id#

uint16_t sl_btmesh_evt_silabs_config_client_model_status_s::model_id

Model ID of model to configure.


Definition at line 3851 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

value#

uint16_t sl_btmesh_evt_silabs_config_client_model_status_s::value

Extended packet size to set, currently 1 to use extended 0 to not


Definition at line 3852 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h