Data structure of the network_pdu_changed event.
Public Attribute Documentation#
max_size#
uint16_t sl_btmesh_evt_silabs_config_server_network_pdu_changed_s::max_size
Max size of packet to be used, in range 29 - 227 bytes.
Definition at line
22196
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h