Data structure of the time_zone_offset_updated event.

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_time_server_time_zone_offset_updated_s::elem_index

Server model element index


Definition at line 16188 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

time_zone_offset_current#

int16_t sl_btmesh_evt_time_server_time_zone_offset_updated_s::time_zone_offset_current

Current local time zone offset. Range is -64 to 191, representing -16 to 47.75 hours.


Definition at line 16189 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

time_zone_offset_new#

int16_t sl_btmesh_evt_time_server_time_zone_offset_updated_s::time_zone_offset_new

Upcoming local time zone offset. Range is -64 to 191, representing -16 to 47.75 hours.


Definition at line 16192 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

tai_of_zone_change#

uint64_t sl_btmesh_evt_time_server_time_zone_offset_updated_s::tai_of_zone_change

Absolute TAI time when the Time Zone Offset will change from Current to New


Definition at line 16195 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h