Data structure of the beacon_status event.

Public Attributes#

uint16_t
uint32_t
uint8_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_config_client_beacon_status_s::result

SL_STATUS_OK if successful. Error code otherwise.


Definition at line 8562 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

handle#

uint32_t sl_btmesh_evt_config_client_beacon_status_s::handle

Request handle


Definition at line 8563 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

value#

uint8_t sl_btmesh_evt_config_client_beacon_status_s::value

Secure network beacon state of the node. Valid values are:

  • 0: Node is not broadcasting secure network beacons

  • 1: Node is broadcasting secure network beacons


Definition at line 8564 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h