Data structure of the bindings_list_end event.

Public Attributes#

uint16_t
uint32_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_config_client_bindings_list_end_s::result

SL_STATUS_OK if successful. Error code otherwise.


Definition at line 8351 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

handle#

uint32_t sl_btmesh_evt_config_client_bindings_list_end_s::handle

Request handle


Definition at line 8352 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h