Data structure of the dcd_data event.

Public Attributes#

uint32_t
uint8_t

Public Attribute Documentation#

handle#

uint32_t sl_btmesh_evt_config_client_dcd_data_s::handle

Request handle


Definition at line 8827 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

page#

uint8_t sl_btmesh_evt_config_client_dcd_data_s::page

Composition data page containing data


Definition at line 8828 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

data#

uint8array sl_btmesh_evt_config_client_dcd_data_s::data

Composition data page contents


Definition at line 8829 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h