Data structure of the friend_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_config_client_friend_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
8738
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
handle#
uint32_t sl_btmesh_evt_config_client_friend_status_s::handle
Request handle
Definition at line
8739
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
value#
uint8_t sl_btmesh_evt_config_client_friend_status_s::value
Friend value to set. Valid values are:
0: Friend feature is not enabled
1: Friend feature is enabled
2: Friend feature is not supported
Definition at line
8740
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h