Data structure of the gatt_proxy_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_config_client_gatt_proxy_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
8614
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
handle#
uint32_t sl_btmesh_evt_config_client_gatt_proxy_status_s::handle
Request handle
Definition at line
8615
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
value#
uint8_t sl_btmesh_evt_config_client_gatt_proxy_status_s::value
GATT proxy value of the node. Valid values are:
0: GATT proxy feature is disabled
1: GATT proxy feature is enabled
2: GATT proxy feature is not supported
Definition at line
8616
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h