Data structure of the heartbeat_pub_status event.

Public Attributes#

uint16_t
uint32_t
uint16_t
uint8_t
uint8_t
uint8_t
uint16_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::result

SL_STATUS_OK if successful. Error code otherwise.


handle#

uint32_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::handle

Request handle


destination_address#

uint16_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::destination_address

Heartbeat publication destination address.


netkey_index#

uint16_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::netkey_index

Index of the network key used to encrypt heartbeat messages


count_log#

uint8_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::count_log

Heartbeat publication count logarithm-of-2 setting


period_log#

uint8_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::period_log

Heartbeat publication period logarithm-of-2 setting


ttl#

uint8_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::ttl

Time-to-live value for heartbeat messages


features#

uint16_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::features

Heartbeat trigger setting