Data structure of the heartbeat_sub_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_config_client_heartbeat_sub_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
8528
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
handle#
uint32_t sl_btmesh_evt_config_client_heartbeat_sub_status_s::handle
Request handle
Definition at line
8530
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
source_address#
uint16_t sl_btmesh_evt_config_client_heartbeat_sub_status_s::source_address
Source address for heartbeat messages
Definition at line
8531
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
destination_address#
uint16_t sl_btmesh_evt_config_client_heartbeat_sub_status_s::destination_address
Destination address for heartbeat messages
Definition at line
8532
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
period_log#
uint8_t sl_btmesh_evt_config_client_heartbeat_sub_status_s::period_log
Heartbeat subscription remaining period logarithm-of-2 value
Definition at line
8533
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
count_log#
uint8_t sl_btmesh_evt_config_client_heartbeat_sub_status_s::count_log
Received heartbeat message count logarithm-of-2 value
Definition at line
8535
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
min_hops#
uint8_t sl_btmesh_evt_config_client_heartbeat_sub_status_s::min_hops
Minimum hop value seen in received heartbeat messages
Definition at line
8537
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
max_hops#
uint8_t sl_btmesh_evt_config_client_heartbeat_sub_status_s::max_hops
Minimum hop value seen in received heartbeat messages
Definition at line
8539
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h