Data structure of the lpn_polltimeout_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_config_client_lpn_polltimeout_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
poll_timeout_ms#
uint32_t sl_btmesh_evt_config_client_lpn_polltimeout_status_s::poll_timeout_ms
Poll timeout value, in milliseconds, for the specified LPN. The value reported is zero if the queried Friend does not have an ongoing friendship with the specified LPN.