Data structure of the netkey_list event.

Public Attributes#

uint32_t

Public Attribute Documentation#

handle#

uint32_t sl_btmesh_evt_config_client_netkey_list_s::handle

Request handle


Definition at line 8179 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

netkey_indices#

uint8array sl_btmesh_evt_config_client_netkey_list_s::netkey_indices

List of network key indices, two bytes per entry


Definition at line 8180 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h