Data structure of the network_transmit_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_config_client_network_transmit_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
transmit_count#
uint8_t sl_btmesh_evt_config_client_network_transmit_status_s::transmit_count
Network transmit count. Valid values range from 1 to 8; default value is 1 (single transmission; no retransmissions).
transmit_interval_ms#
uint16_t sl_btmesh_evt_config_client_network_transmit_status_s::transmit_interval_ms
Network transmit interval in milliseconds. Valid values range from 10 ms to 320 ms, with a resolution of 10 ms. The value will be zero if the transmission count is set to one.