Data structure of the partial_block_report_tx_complete event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_mbt_server_partial_block_report_tx_complete_s::elem_index
The server model element index.
Definition at line
11412
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
num_requested_chunks#
uint16_t sl_btmesh_evt_mbt_server_partial_block_report_tx_complete_s::num_requested_chunks
Number of requested chunks.
Definition at line
11413
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
requested_chunks#
uint8array sl_btmesh_evt_mbt_server_partial_block_report_tx_complete_s::requested_chunks
The array of requested chunks in little-endian uint16 format.
Definition at line
11414
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h