Data structure of the config_get event.

Public Attributes#

uint16_t
uint16_t

Public Attribute Documentation#

netkey_index#

uint16_t sl_btmesh_evt_node_config_get_s::netkey_index

The network key index of the network to which the command applies. 0xffff for node-wide states.


Definition at line 470 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

id#

uint16_t sl_btmesh_evt_node_config_get_s::id

Enum sl_btmesh_node_config_state_t. Specifies to which State the command applies


Definition at line 472 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h