Data structure of the heartbeat_start event.
Public Attribute Documentation#
src_addr#
uint16_t sl_btmesh_evt_node_heartbeat_start_s::src_addr
Source address for the heartbeat message
Definition at line
832
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
dst_addr#
uint16_t sl_btmesh_evt_node_heartbeat_start_s::dst_addr
Destination address for the heartbeat message
Definition at line
833
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
period_sec#
uint32_t sl_btmesh_evt_node_heartbeat_start_s::period_sec
Heartbeat subscription period in seconds.
Definition at line
834
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h