Data structure of the initialized event.
Public Attribute Documentation#
provisioned#
uint8_t sl_btmesh_evt_node_initialized_s::provisioned
1 if node is provisioned into a network, 0 if unprovisioned.
address#
uint16_t sl_btmesh_evt_node_initialized_s::address
Unicast address of the primary element of the node. Ignored if unprovisioned. Secondary elements have been assigned sequential unicast addresses following the primary element address.
iv_index#
uint32_t sl_btmesh_evt_node_initialized_s::iv_index
IV index for the first network of the node, ignore if unprovisioned.