Data structure of the start_received event.

Public Attribute Documentation#

algorithm#

uint8_t sl_btmesh_evt_node_start_received_s::algorithm

Selected provisioning algorithm


Definition at line 1004 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

public_key#

uint8_t sl_btmesh_evt_node_start_received_s::public_key

Selected OOB public key


Definition at line 1005 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

authentication_method#

uint8_t sl_btmesh_evt_node_start_received_s::authentication_method

Selected authentication method


Definition at line 1006 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

authentication_action#

uint8_t sl_btmesh_evt_node_start_received_s::authentication_action

Selected authentication action


Definition at line 1007 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

authentication_size#

uint8_t sl_btmesh_evt_node_start_received_s::authentication_size

Selected authentication size


Definition at line 1008 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h