Data structure of the capabilities event.

Public Attribute Documentation#

uuid#

uuid_128 sl_btmesh_evt_prov_capabilities_s::uuid

UUID of the device being provisioned


elements#

uint8_t sl_btmesh_evt_prov_capabilities_s::elements

Number of elements supported by the device


algorithms#

uint16_t sl_btmesh_evt_prov_capabilities_s::algorithms

Supported algorithms and other capabilities.


pkey_type#

uint8_t sl_btmesh_evt_prov_capabilities_s::pkey_type

Supported public key types


static_oob_type#

uint8_t sl_btmesh_evt_prov_capabilities_s::static_oob_type

Supported static OOB Types


ouput_oob_size#

uint8_t sl_btmesh_evt_prov_capabilities_s::ouput_oob_size

Maximum size of Output OOB supported


output_oob_action#

uint16_t sl_btmesh_evt_prov_capabilities_s::output_oob_action

Supported Output OOB Actions


input_oob_size#

uint8_t sl_btmesh_evt_prov_capabilities_s::input_oob_size

Maximum size of input OOB supported


intput_oob_action#

uint16_t sl_btmesh_evt_prov_capabilities_s::intput_oob_action

Supported input OOB Actions