Data structure of the device_provisioned event.

Public Attributes#

uint16_t

Public Attribute Documentation#

address#

uint16_t sl_btmesh_evt_prov_device_provisioned_s::address

Address assigned to the node's primary element. If the node has multiple elements, they have been assigned an address in a consecutive sequence following the primary element address.


Definition at line 2324 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

uuid#

uuid_128 sl_btmesh_evt_prov_device_provisioned_s::uuid

UUID of the device


Definition at line 2328 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h