Data structure of the key_refresh_complete event.

Public Attributes#

uint16_t
uint16_t

Public Attribute Documentation#

key#

uint16_t sl_btmesh_evt_prov_key_refresh_complete_s::key

Network key index


Definition at line 2565 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

result#

uint16_t sl_btmesh_evt_prov_key_refresh_complete_s::result

SL_STATUS_OK if successful. Error code otherwise.


Definition at line 2566 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h