Data structure of the oob_display_input event.
Public Attribute Documentation#
uuid#
uuid_128 sl_btmesh_evt_prov_oob_display_input_s::uuid
UUID of the device
Definition at line
2437
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
input_action#
uint8_t sl_btmesh_evt_prov_oob_display_input_s::input_action
Enum sl_btmesh_node_oob_input_action_t. Input action type
Definition at line
2438
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
input_size#
uint8_t sl_btmesh_evt_prov_oob_display_input_s::input_size
Number of digits or characters
Definition at line
2440
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
data#
uint8array sl_btmesh_evt_prov_oob_display_input_s::data
Raw 16-byte array
Definition at line
2441
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h