Data structure of the provisioning_failed event.
Public Attribute Documentation#
reason#
uint8_t sl_btmesh_evt_prov_provisioning_failed_s::reason
Reason for failure. Values are as follows:
0: Link closed
1: Invalid PDU
2: Invalid PDU format
3: Unexpected PDU
4: Confirmation failed
5: Out of resources
6: Decryption failed
7: Unexpected error
8: Unable to assign address
Definition at line
2293
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
uuid#
uuid_128 sl_btmesh_evt_prov_provisioning_failed_s::uuid
UUID of the device
Definition at line
2303
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h