Data structure of the column_status event.

Public Attributes#

uint16_t
uint16_t
uint8_t
uint16_t

Public Attribute Documentation#

client_address#

uint16_t sl_btmesh_evt_sensor_client_column_status_s::client_address

Destination client model address


Definition at line 12551 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_sensor_client_column_status_s::elem_index

Client model element index


Definition at line 12552 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_sensor_client_column_status_s::server_address

Source server model address


Definition at line 12553 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_sensor_client_column_status_s::appkey_index

The application key index to use


Definition at line 12554 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

flags#

uint8_t sl_btmesh_evt_sensor_client_column_status_s::flags

No flags defined currently


Definition at line 12555 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

property_id#

uint16_t sl_btmesh_evt_sensor_client_column_status_s::property_id

Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.


Definition at line 12556 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

sensor_data#

uint8array sl_btmesh_evt_sensor_client_column_status_s::sensor_data

Byte array containing the serialized Sensor Series Column state in the following format:

  • Sensor Raw Value X, variable length raw value representing the left corner of a column

  • Sensor Column Width, variable length raw value representing the width of the column

  • Sensor Raw Value Y, variable length raw value representing the height of the column

If the requested Property ID or column ID does not exist at the server elements, the reply status message contains only these two fields, omitting column width and height values.


Definition at line 12559 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h