Data structure of the time_role_status event.

Public Attributes#

uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

client_address#

uint16_t sl_btmesh_evt_time_client_time_role_status_s::client_address

Client address


elem_index#

uint16_t sl_btmesh_evt_time_client_time_role_status_s::elem_index

Client model element index


server_address#

uint16_t sl_btmesh_evt_time_client_time_role_status_s::server_address

Unicast address of the server


appkey_index#

uint16_t sl_btmesh_evt_time_client_time_role_status_s::appkey_index

App key index.


time_role#

uint8_t sl_btmesh_evt_time_client_time_role_status_s::time_role

The Time Role for the element