Data structure of the time_status event.
Public Attribute Documentation#
client_address#
uint16_t sl_btmesh_evt_time_client_time_status_s::client_address
Client address
Definition at line
16558
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_time_client_time_status_s::elem_index
Client model element index
Definition at line
16559
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_time_client_time_status_s::server_address
Unicast address of the server
Definition at line
16560
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_time_client_time_status_s::appkey_index
App key index.
Definition at line
16561
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
tai_seconds#
uint64_t sl_btmesh_evt_time_client_time_status_s::tai_seconds
The current TAI time in seconds
Definition at line
16562
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
subsecond#
uint8_t sl_btmesh_evt_time_client_time_status_s::subsecond
The sub-second time in units of 1/256th second
Definition at line
16563
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
uncertainty#
uint8_t sl_btmesh_evt_time_client_time_status_s::uncertainty
The estimated uncertainty in 10-millisecond steps
Definition at line
16564
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
time_authority
uint8_t sl_btmesh_evt_time_client_time_status_s::time_authority
0 = No Time Authority, 1 = Time Authority
Definition at line
16566
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
tai_utc_delta#
int32_t sl_btmesh_evt_time_client_time_status_s::tai_utc_delta
Current difference between TAI and UTC in seconds. Range is -255 to 32512.
Definition at line
16567
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
time_zone_offset#
int16_t sl_btmesh_evt_time_client_time_status_s::time_zone_offset
The local time zone offset in 15-minute increments. Range is -64 to 191, representing -16 to 47.75 hours.
Definition at line
16569
of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h