Data structure of the transfer_start_req event.

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_mbt_server_transfer_start_req_s::elem_index

The server model element index.


Definition at line 11345 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_mbt_server_transfer_start_req_s::client_address

The address of the MBT Client.


Definition at line 11346 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

blob_id#

sl_bt_uuid_64_t sl_btmesh_evt_mbt_server_transfer_start_req_s::blob_id

The ID of the BLOB.


Definition at line 11347 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

blob_size#

uint32_t sl_btmesh_evt_mbt_server_transfer_start_req_s::blob_size

The size of the BLOB.


Definition at line 11348 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

block_size_log#

uint8_t sl_btmesh_evt_mbt_server_transfer_start_req_s::block_size_log

The block size as an exponent n in 2^n.


Definition at line 11349 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

transfer_mode#

uint8_t sl_btmesh_evt_mbt_server_transfer_start_req_s::transfer_mode

Transfer mode: 1 = Push Mode (client-driven), 2 = Pull Mode (server-driven).


Definition at line 11350 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h