Data structure of the default_ttl_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_config_client_default_ttl_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
8667
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
handle#
uint32_t sl_btmesh_evt_config_client_default_ttl_status_s::handle
Request handle
Definition at line
8668
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
value#
uint8_t sl_btmesh_evt_config_client_default_ttl_status_s::value
Default TTL value. Valid value range is from 2 to 127 for relayed PDUs, and 0 to indicate non-relayed PDUs.
Definition at line
8669
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h