Data structure of the identity_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_config_client_identity_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
8788
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
handle#
uint32_t sl_btmesh_evt_config_client_identity_status_s::handle
Request handle
Definition at line
8789
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
value#
uint8_t sl_btmesh_evt_config_client_identity_status_s::value
Identity state of the node for the used network index. Valid values are as follows:
0: Node identity advertising is disabled
1: Node identity advertising is enabled
2: Node identity advertising is not supported
Definition at line
8790
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h