Data structure of the lpn_polltimeout_status event.

Public Attributes#

uint16_t
uint32_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_config_client_lpn_polltimeout_status_s::result

SL_STATUS_OK if successful. Error code otherwise.


Definition at line 8872 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

handle#

uint32_t sl_btmesh_evt_config_client_lpn_polltimeout_status_s::handle

Request handle


Definition at line 8874 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

poll_timeout_ms#

uint32_t sl_btmesh_evt_config_client_lpn_polltimeout_status_s::poll_timeout_ms

Poll timeout value, in milliseconds, for the specified LPN. The value reported is zero if the queried Friend does not have an ongoing friendship with the specified LPN.


Definition at line 8875 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h